Hi, experts.
I have a problem to encode 2048 * 1536 resolutions with h264 codec.
During the test kernel panic or block come in 15 minutes.
When I set 640 * 480 encode with h264 it is working fine. But over the 640 * 480, the kernel panic or block comes.
And if I test 1280 * 1024 encoding with MPEG4 and 2048*1536 with Mjpeg works fine.
Kernel Block comes at VIDENC1_process() and Kernel panic log as below.
Unable to handle kernel paging request at virtual address ba043e60
pgd = c0004000
Internal error: Oops: 5 [#1]
Modules linked in: sbull iscsi_tcp libiscsi scsi_transport_iscsi ppp_deflate ppp_async ppp_synctty ppp_generic slhc tun loop nfsd exportfs nls_utf8 nls_ascii sha1 md5 des deflate crc32c cfq_iosched deadline_iosched libcrc32c crc_ccitt dm365mmap irqk edmak cmemk drv csl
CPU: 0
PC is at read_cycles+0x24/0x38
LR is at getnstimeofday+0x50/0x1ac
pc : [<c0046f14>] lr : [<c0059608>] Not tainted
sp : c0359da8 ip : c0359db8 fp : c0359db4 r10: c03d8cf4 r9 : c03d7cb0 r8 : c0359e18 r7 : 00000093 r6 : 00056508 r5 : c0359e18 r4 : 00056508 r3 : ba043e60 r2 : 00000001 r1 : 245bdc80 r0 : 386eaf51
Flags: nzcv IRQs off FIQs on Mode SVC_32 Segment kernel
Unable to handle kernel paging request at virtual address ba043e60 pgd = c0004000 [ba043e60] *pgd=00000000 Internal error: Oops: 5 [#1] Modules linked in: sbull iscsi_tcp libiscsi scsi_transport_iscsi ppp_deflate ppp_async ppp_synctty ppp_generic slhc tun loop nfsd exportfs nls_utf8 nls_ascii sha1 md5 des deflate crc32c cfq_iosched deadline_iosched libcrc32c crc_ccitt dm365mmap irqk edmak cmemk drv csl CPU: 0 PC is at read_cycles+0x24/0x38 LR is at getnstimeofday+0x50/0x1ac pc : [<c0046f14>] lr : [<c0059608>] Not tainted sp : c0359da8 ip : c0359db8 fp : c0359db4 r10: c03d8cf4 r9 : c03d7cb0 r8 : c0359e18 r7 : 00000093 r6 : 00056508 r5 : c0359e18 r4 : 00056508 r3 : ba043e60 r2 : 00000001 r1 : 245bdc80 r0 : 386eaf51 Flags: nzcv IRQs off FIQs on Mode SVC_32 Segment kernel Control: 5317F Table: 82378000 DAC: 00000017 Process swapper (pid: 0, stack limit = 0xc0358258) Stack: (0xc0359da8 to 0xc035a000) 9da0: c0359df4 c0359db8 c0059608 c0046f00 c0359e00 c03d7cc0 9dc0: 00000000 00000000 c035db20 00056508 c0359e18 c03d7cc0 c03d7ca0 258e555e 9de0: 00000374 00000000 c0359e14 c0359df8 c006894c c00595c8 c0359e38 00000374 9e00: 24f5f9a0 00000374 c0359e34 c0359e18 c00689a0 c0068938 386eaf51 245bdc80 9e20: 00989680 258e555e c0359e64 c0359e38 c006ab7c c0068994 c0359e64 c0359e48 9e40: c03631c0 c0363170 24f5f9a0 00000374 258e555e c0358000 c0359eac c0359e68 9e60: c006947c c006ab68 24f5f9a0 00000374 0000103d 00000000 24f5f9a0 00000374 9e80: 00000000 00010002 c0358000 c036173c c036173c 00000000 00000020 c0359f40 9ea0: c0359ebc c0359eb0 c0046e58 c006929c c0359ef4 c0359ec0 c00732ec c0046e4c 9ec0: c0054468 00000000 00000020 c035a800 c0358000 00000020 c036173c c0359f40 9ee0: c0358000 c03da998 c0359f1c c0359ef8 c0074f3c c0073224 00000020 c035a800 9f00: c0359f40 00000002 00000001 80030f00 c0359f3c c0359f20 c0038bc0 c0074e34 9f20: c0f51200 ffffffff fbc48000 c0039638 c0359f94 c0359f40 c0037a04 c0038b90 9f40: 00000000 0005317f 0005217f 60000013 c0358000 c0039638 c0039638 c03d184c 9f60: 80030f34 41069265 80030f00 c0359f94 c0359f98 c0359f88 c0039688 c0039694 9f80: 60000013 ffffffff c0359fb4 c0359f98 c00393d0 c0039648 c0358000 c03d13fc 9fa0: c035e804 c03fb760 c0359fcc c0359fb8 c0037300 c00393a4 c035e804 c03dabb4 9fc0: c0359ff4 c0359fd0 c00088dc c00372b8 c00083b4 00000000 00000000 c03d1928 9fe0: 00053175 c03d18c4 00000000 c0359ff8 80008030 c00086d0 00000000 00000000 Backtrace: [<c0046ef0>] (read_cycles+0x0/0x38) from [<c0059608>] (getnstimeofday+0x50/0x1ac) [<c00595b8>] (getnstimeofday+0x0/0x1ac) from [<c006894c>] (ktime_get_ts+0x24/0x5c) [<c0068928>] (ktime_get_ts+0x0/0x5c) from [<c00689a0>] (ktime_get+0x1c/0x34) r7 = 00000374 r6 = 24F5F9A0 r5 = 00000374 r4 = C0359E38 [<c0068984>] (ktime_get+0x0/0x34) from [<c006ab7c>] (clockevents_set_next_event+0x24/0x12c) r4 = 258E555E [<c006ab58>] (clockevents_set_next_event+0x0/0x12c) from [<c006947c>] (hrtimer_interrupt+0x1f0/0x230) [<c006928c>] (hrtimer_interrupt+0x0/0x230) from [<c0046e58>] (timer_interrupt+0x1c/0x28) [<c0046e3c>] (timer_interrupt+0x0/0x28) from [<c00732ec>] (handle_IRQ_event+0xd8/0x1c4) [<c0073214>] (handle_IRQ_event+0x0/0x1c4) from [<c0074f3c>] (handle_edge_irq+0x118/0x1cc) [<c0074e24>] (handle_edge_irq+0x0/0x1cc) from [<c0038bc0>] (asm_do_IRQ+0x40/0x50) [<c0038b80>] (asm_do_IRQ+0x0/0x50) from [<c0037a04>] (__irq_svc+0x44/0x70) r6 = C0039638 r5 = FBC48000 r4 = FFFFFFFF [<c0039638>] (default_idle+0x0/0x64) from [<c00393d0>] (cpu_idle+0x3c/0x94) [<c0039394>] (cpu_idle+0x0/0x94) from [<c0037300>] (rest_init+0x58/0x64) r7 = C03FB760 r6 = C035E804 r5 = C03D13FC r4 = C0358000 [<c00372a8>] (rest_init+0x0/0x64) from [<c00088dc>] (start_kernel+0x21c/0x27c) r4 = C03DABB4 [<c00086c0>] (start_kernel+0x0/0x27c) from [<80008030>] (0x80008030) Code: e59f3018 e7933102 e5933014 e28334fa (e5930000) <1>Unable to handle kernel NULL pointer dereference at virtual address 00000000 pgd = c0004000 [00000000] *pgd=00000000 Internal error: Oops: 817 [#2] Modules linked in: sbull iscsi_tcp libiscsi scsi_transport_iscsi ppp_deflate ppp_async ppp_synctty ppp_generic slhc tun loop nfsd exportfs nls_utf8 nls_ascii sha1 md5 des deflate crc32c cfq_iosched deadline_iosched libcrc32c crc_ccitt dm365mmap irqk edmak cmemk drv csl CPU: 0 PC is at do_exit+0x58/0xa24 LR is at compat_up_read+0x10/0x14 pc : [<c0051798>] lr : [<c00694f4>] Not tainted sp : c0359bf8 ip : 00000000 fp : c0359c14 r10: c030b730 r9 : 00000000 r8 : 0000000b r7 : 00000000 r6 : 00000001 r5 : c035db20 r4 : c0358000 r3 : 00000000 r2 : 00010002 r1 : c0361d00 r0 : 00000000 Flags: nzCv IRQs on FIQs on Mode SVC_32 Segment kernel Control: 5317F Table: 82378000 DAC: 00000017 Process swapper (pid: 0, stack limit = 0xc0358258) Stack: (0xc0359bf8 to 0xc035a000) 9be0: c030b730 c0359c2c 9c00: 60000093 c0359c18 c0359c2c c0359c18 c003c5bc c0051750 00000000 00000008 9c20: c0359c4c c0359c30 c003eb20 c003c24c ffffffff c035eb08 00000005 c035db20 9c40: c0359c94 c0359c50 c003edc4 c003eac4 00000000 c21a6480 a0000013 c04db1c0 9c60: 00000005 00000000 c0359c94 ffffffff c035eb08 00000005 c0359d60 ba043e60 9c80: 40000093 c03d8cf4 c0359cac c0359c98 c003ee94 c003eb40 c04db1c0 ffffffff 9ca0: c0359d5c c0359cb0 c003ef84 c003ee88 c02b2078 c21a6480 c04db1c0 c04db1c0 9cc0: c21a6480 00000014 c04db1f0 c0581854 c0359d0c c0359ce0 c02ae830 c02a91ac 9ce0: c0359d2c c0358000 c21a6480 c04db1c0 c21a6480 7a01a8c0 c035ca14 c0581854 9d00: c0359d4c c0359d10 c02b509c c02ae70c c03d2780 c0635c20 c0359d3c c0359d28 9d20: c0048700 c0048614 c0635c20 c03d2780 c0359d5c c0359d40 c00487a0 ffffffff 9d40: c0359d94 00056508 00000093 c0359e18 c0359db4 c0359d60 c00379ac c003ef58 9d60: 386eaf51 245bdc80 00000001 ba043e60 00056508 c0359e18 00056508 00000093 9d80: c0359e18 c03d7cb0 c03d8cf4 c0359db4 c0359db8 c0359da8 c0059608 c0046f14 9da0: 00000093 ffffffff c0359df4 c0359db8 c0059608 c0046f00 c0359e00 c03d7cc0 9dc0: 00000000 00000000 c035db20 00056508 c0359e18 c03d7cc0 c03d7ca0 258e555e 9de0: 00000374 00000000 c0359e14 c0359df8 c006894c c00595c8 c0359e38 00000374 9e00: 24f5f9a0 00000374 c0359e34 c0359e18 c00689a0 c0068938 386eaf51 245bdc80 9e20: 00989680 258e555e c0359e64 c0359e38 c006ab7c c0068994 c0359e64 c0359e48 9e40: c03631c0 c0363170 24f5f9a0 00000374 258e555e c0358000 c0359eac c0359e68 9e60: c006947c c006ab68 24f5f9a0 00000374 0000103d 00000000 24f5f9a0 00000374 9e80: 00000000 00010002 c0358000 c036173c c036173c 00000000 00000020 c0359f40 9ea0: c0359ebc c0359eb0 c0046e58 c006929c c0359ef4 c0359ec0 c00732ec c0046e4c 9ec0: c0054468 00000000 00000020 c035a800 c0358000 00000020 c036173c c0359f40 9ee0: c0358000 c03da998 c0359f1c c0359ef8 c0074f3c c0073224 00000020 c035a800 9f00: c0359f40 00000002 00000001 80030f00 c0359f3c c0359f20 c0038bc0 c0074e34 9f20: c0f51200 ffffffff fbc48000 c0039638 c0359f94 c0359f40 c0037a04 c0038b90 9f40: 00000000 0005317f 0005217f 60000013 c0358000 c0039638 c0039638 c03d184c 9f60: 80030f34 41069265 80030f00 c0359f94 c0359f98 c0359f88 c0039688 c0039694 9f80: 60000013 ffffffff c0359fb4 c0359f98 c00393d0 c0039648 c0358000 c03d13fc 9fa0: c035e804 c03fb760 c0359fcc c0359fb8 c0037300 c00393a4 c035e804 c03dabb4 9fc0: c0359ff4 c0359fd0 c00088dc c00372b8 c00083b4 00000000 00000000 c03d1928 9fe0: 00053175 c03d18c4 00000000 c0359ff8 80008030 c00086d0 00000000 00000000 Backtrace: [<c0051740>] (do_exit+0x0/0xa24) from [<c003c5bc>] (die+0x380/0x3e8) [<c003c23c>] (die+0x0/0x3e8) from [<c003eb20>] (__do_kernel_fault+0x6c/0x7c) [<c003eab4>] (__do_kernel_fault+0x0/0x7c) from [<c003edc4>] (do_page_fault+0x294/0x2c4) r7 = C035DB20 r6 = 00000005 r5 = C035EB08 r4 = FFFFFFFF [<c003eb30>] (do_page_fault+0x0/0x2c4) from [<c003ee94>] (do_translation_fault+0x1c/0xb4) [<c003ee78>] (do_translation_fault+0x0/0xb4) from [<c003ef84>] (do_DataAbort+0x3c/0xa0) r4 = FFFFFFFF [<c003ef48>] (do_DataAbort+0x0/0xa0) from [<c00379ac>] (__dabt_svc+0x4c/0x60) r8 = C0359E18 r7 = 00000093 r6 = 00056508 r5 = C0359D94 r4 = FFFFFFFF [<c0046ef0>] (read_cycles+0x0/0x38) from [<c0059608>] (getnstimeofday+0x50/0x1ac) [<c00595b8>] (getnstimeofday+0x0/0x1ac) from [<c006894c>] (ktime_get_ts+0x24/0x5c) [<c0068928>] (ktime_get_ts+0x0/0x5c) from [<c00689a0>] (ktime_get+0x1c/0x34) r7 = 00000374 r6 = 24F5F9A0 r5 = 00000374 r4 = C0359E38 [<c0068984>] (ktime_get+0x0/0x34) from [<c006ab7c>] (clockevents_set_next_event+0x24/0x12c) r4 = 258E555E [<c006ab58>] (clockevents_set_next_event+0x0/0x12c) from [<c006947c>] (hrtimer_interrupt+0x1f0/0x230) [<c006928c>] (hrtimer_interrupt+0x0/0x230) from [<c0046e58>] (timer_interrupt+0x1c/0x28) [<c0046e3c>] (timer_interrupt+0x0/0x28) from [<c00732ec>] (handle_IRQ_event+0xd8/0x1c4) [<c0073214>] (handle_IRQ_event+0x0/0x1c4) from [<c0074f3c>] (handle_edge_irq+0x118/0x1cc) [<c0074e24>] (handle_edge_irq+0x0/0x1cc) from [<c0038bc0>] (asm_do_IRQ+0x40/0x50) [<c0038b80>] (asm_do_IRQ+0x0/0x50) from [<c0037a04>] (__irq_svc+0x44/0x70) r6 = C0039638 r5 = FBC48000 r4 = FFFFFFFF [<c0039638>] (default_idle+0x0/0x64) from [<c00393d0>] (cpu_idle+0x3c/0x94) [<c0039394>] (cpu_idle+0x0/0x94) from [<c0037300>] (rest_init+0x58/0x64) r7 = C03FB760 r6 = C035E804 r5 = C03D13FC r4 = C0358000 [<c00372a8>] (rest_init+0x0/0x64) from [<c00088dc>] (start_kernel+0x21c/0x27c) r4 = C03DABB4 [<c00086c0>] (start_kernel+0x0/0x27c) from [<80008030>] (0x80008030) Code: e3c334ff e3c330ff e3530000 13a03000 (15833000)
I attached the full error log.
please let me know how to solve this error.
Best regards.
Jay.