Other Parts Discussed in Thread: DM3730
Currently we use 26M crystal and it works fine in our DM3730 platform. (x-loader 1.5.1, 2.6.37 kernel).
Since we need to fix the USB clock issue, we had to change the 26MHz to 38.4Mhz as TI recommend.
It seems x-loader will detect crystal input automatically and we donn't need to change anything.
But we failed and we cann't see the right serial output in x-loader because of the wrong baudrate.
What others settings we should do for 38.4M crystal input?
Regards,