Hi Ti folks,
There is a error in build of platform library in installation folders of PDK 6678 [version pdk_C6678_1_0_0_21]
evm6678.c
below print statement is incorrect [when PLATFORM_DEBUG is set to 1]
===================================================================error 1
line 554
IFPRINT(platform_write("DSP core #%d cannot set DDR3 PLL \n",,2,,,DNUM));
===================================================================error 2
line 414
IFPRINT(platform_write("DSP core #%d cannot set PA PLL \n",,2,,,DNUM));
the above errors are in both linux and windows version
===================================================================error 3
below error i see only in linux version of platform library build
<PDK INSTALLATION PATH>/packages//ti/platform/evmc6678l/platform_lib/include/platform_internal.h", line 121: fatal error: #error You must enable PLATFORM_WRITE to turn on DEBUG
1 fatal error detected in the compilation of "src/evm66x_i2c.c".
Compilation terminated.
This error comes for #ifdef _PLATFORM_LITE_ case
===================================================================
Thanks
RC Reddy