I notice in the C6678 EVB schematic, that the 1.8V is split into 2 voltage regulators (TPS73701). 1 is always enabled (C6678 TSIP, JTAG, GPIO Bootmode) and the other regulator is enabled by FPGA for power sequencing.
Could I use 1 voltage regulator (TPS73701) for C6678 (C6678 TSIP, JTAG, GPIO Bootmode as well as other C66 peripherals that uses 1.8V) and that regulator will be controlled by power sequencing. Would I still be able to JTAG into C6678 if I use 1 voltage regulator instead of 2.