This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with Getting Started With C6Run On Beagleboard

Hi all,

Has anyone followed the guide at the following link? 

http://processors.wiki.ti.com/index.php/Getting_Started_With_C6Run_On_Beagleboard

I have a problem with the sections "Open Embedded and angstrom setup" and "Building base image for beaglboard" . In "Open Embedded and angstrom" section the comand 

  ~/Git$ git clone git://gitorious.org/angstrom/angstrom-setup-scripts.git angstrom-setup-scripts
result obsolete and I followed the guide at site below
http://www.angstrom-distribution.org/building-angstrom
 with the link updated as
  ~/Git$ git clone git://github.com/Angstrom-distribution/setup-scripts.git
I followed the steps but then I am not the directory "angstrom-setup-scripts/build/tmp-angstrom_2008_1/deploy/glibc/images/beagleboard" is created after running the command
~/Git/angstrom-setup-scripts$ bitbake base-image console-image

After the command bitbake does not create the directory and then have a problem then to select the kernel from this folder.

I have already tried to install the TI C6000 Code Generation tools and C6Run but for a correct compilation requires the directory 

"angstrom-setup-scripts/build/tmp-angstrom_2008_1/deploy/glibc/images/beagleboard"
Has anyone done these steps? May attach the folder build.zip?

Maurizio