This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

help : about DSPLIB

I wonder the type of "DATA" in the DSPLIB.   Is it Q. 15 or Q15 ?

I see that  DATA is defined as short type in the related material.

I think the short type is equal to Q15 type.

but from the routine using the DPSLIB in the ccs installing folder , the result is right if wo consider "DATA" as "Q. 15",and it is wrong if wo consider "DATA" as "short".

So i don't know how can I define the variable in a c program if i want to use the DSPLIB.

Thank you very much.