Hello,
On my design, I use the TMS320C6671ACYPA with 4 DDR3 (128M * 16bits) and I do not use ECC function.
How should I polarize the signals DDRCB [7:0] and the signals DDRDQS8P/N?.
Thanks
Best Regards
Pascal
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
On my design, I use the TMS320C6671ACYPA with 4 DDR3 (128M * 16bits) and I do not use ECC function.
How should I polarize the signals DDRCB [7:0] and the signals DDRDQS8P/N?.
Thanks
Best Regards
Pascal
Pascal,
The unused DDRCB[7:0] pins can be left unconnected when ECC is not needed. This is stated in section "7.8.4 Unused DDR3 Pin Requirement" of the Hardware Design Guide for KeyStone I Devices Application Report (SPRABI2B). The DDR3 Design Requirements for KeyStone Devices Application Report (SPRABI1A) also has implementation examples.
Tom