Other Parts Discussed in Thread: TMS320C6657
While waiting for initial build of our custom hardware (which has a C6657 DSP on it), I've developed and tested a good portion of the software using a TMDXEVM6657LE evaluation card. With that card, I built with the ti.platforms.evm6657 platform, which I used mainly to communicate with SRIO and with the UART. Now that our hardware is in house, I am no longer using the eval card exclusively. Our hardware is slightly different than what was on the eval card, so ti.platforms.evm6657 is no longer the correct platform to use.
My question is: How do I port the evm6657 platform to work on our hardware?
Initially, all I need to do is modify DDR3 PLL parameters, and set up the EMIF16 bus for our needs.
This is what I tried:
I imported the platform_lib project into my workspace. So that I wouldn't modify the original code (I need it, because I still do basic development on the eval card), I copied the files to my workspace. After setting up include folders to be correct, I got the library to compile. I added it as a linked-file to the app project, and it appeared to link.
When running the app under CCS debug on our hardware, it didn't know where to find the source files (which sent up a red flag). I pointed it to the source files in my workspace, and the debugger displayed the code correctly. Using CCS, we modified PLL variables, and we got our DDR3 SDRAM to work.
The next thing I did was to modify my copy of the platform library to use our PLL values. I didn't delete the original code; instead, I simply #ifdef'd the old code out and the new code in. I set a breakpoint in the DDR init code, and ran it. When the breakpoint hit, CCS displayed the source file, but it was on the wrong line (an even more obvious red flag). It was apparent that the platform library that was linked into my app was the original (with the original source-file line numbers), and that the new one was not linked at all.
I'm sure that this has something to with all the XDC and RTSC stuff that CCS uses. I don't understand all of that, and our schedule does not allow time for me to figure it out. Hopefully, someone can point me to some clear, concise documentation that describes what I need to do to make this work.