This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RGB Display mapping output pin modify

Other Parts Discussed in Thread: 4460

Hi~

We used Pandaboard (OMAP 4460) to develop.

And we want to bring up 18 bit RGB panel .

Could we assign the RGB output pin by driver?

EX :             R[5:0] =>D[5:0]    G[5:0]=>D[6:11]   B[5:0] => D[12:17]

assign to     R[5:0] =>D[5:0]    G[5:0]=>D[13:8]   B[5:0] => D[21:16]

 

thanks.

 

  • William,

    Check the panel datasheet. It will give the order in which it expects the data. If you still doubt, share the datasheet.

  • Dear Thomas

    We have a PCB board to connect panel and PandaBoard.( RGB pin to Socket )

    The PCB board pin define not match pandaboard output.(Design problem)

    Pin to Pin connect.

    Pandaboard D[23:0]=PCB board D[23:0]=>Panel

    Output 18 bit RGB

    PandaBoard D[5:0] ( R[5:0] )         =>  PCBboard D[5:0]     => Not used => Panel

    PandaBoard D[11:6] ( G[5:0])        =>  PCBboard D[11:6]    =>  R[5:0] => Panel

    PandaBoard D[17:12] (B[5:0] )      =>  PCBboard D[17:12]   =>  G[5:0] => Panel

    PandaBoard D[23:17] (XXXXXX)    =>PCBboard [23:18]      =>  B[5:0] => Panel

     

    Could We modify PandaBoard RGB output pin (Ex: 18bit D[17:0] to D[23:6])??

    thank you.

  • Hi Wu

    If the pandaboard RGB output you refer is dispc2_data[0:23] then you cannot change the order of the pins.

    Also, if you check the 4460 TRM Figure 10-17 you'll see that data[0:5] is blue, data[6:11] green and data[12:17] is red.

    Regards

    Rafael

  • Hi Rafael

     

    yes , you are right. D[5:0] is Blue.

    Thanks your support.