Other Parts Discussed in Thread: OMAPL138
Hi,everyone!
I'm a newcomer.I've really puzzled over the question for a long time.I've tried to rebuilt my Uimage ,and reinstalled my ubuntu 10.04,but still,it stucks here:"uncompressing linux..."
I've set the board starting from NANDFLASH.my cpu is OMAPL138,and my board is SEED_DEC138,and here is my uboot environment:
U-Boot > printenv
bootdelay=3
baudrate=115200
bootfile="uImage"
ethaddr=0a:c1:a8:15:fa:c0
ethact=
ip=10.108.51.101
filesize=F60000
fileaddr=C1180000
serverip=192.168.253.77
ipaddr=192.168.253.123
bootargs=mem=128M console=ttyS0,115200n8 root=/dev/nfs
bootcmd=tftp 0xc0700000 uImage; bootm
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 2009.01 (Jan 06 2010 - 11:01:54)
the upper red line is a little strange ,I guess it's from my last setting,but I guess it has nothing to do with the problem since the board can download uImage successfully through tftp.
problems occured after I reset the board:
Environment size: 356/131068 bytes
U-Boot >
U-Boot 2009.01 (Jan 06 2010 - 11:01:54)
I2C: ready
DRAM: 64 MB
NAND: NAND device: Manufacturer ID: 0xec, Chip ID: 0xdc (Samsung NAND 512MiB 3)
Bad block table found at page 262080, version 0x01
Bad block table found at page 262016, version 0x01
nand_read_bbt: Bad block at 0x11860000
nand_read_bbt: Bad block at 0x1b7a0000
512 MiB
In: serial
Out: serial
Err: serial
ARM Clock : 300000000 Hz
DDR Clock : 150000000 Hz
Net: More than one PHY detected.
Hit any key to stop autoboot: 0
Using device
TFTP from server 192.168.253.77; our IP address is 192.168.253.123
Filename 'uImage'.
Load address: 0xc0700000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################
done
Bytes transferred = 1832092 (1bf49c hex)
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-2.6.32-rc6
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1832028 Bytes = 1.7 MB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux.............................................................
then it stucks here,nothing happens.