This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiling Error with c6runlib-ar



Hi,

I tried to wirte a simple program for my C674x on my EMV8618, what simply calculates the primes until a given number.

The code looks like:

void prim(int untill, int* a){
    
    int i,j,n;
    
    n = 0;
    
    for(i=1;i <= untill; ++i){
        for(j=1; j<=i;++i){
            if(i%j == 0){
                if(i == j && j != 1){
                    a[n] = i;
                    ++n;
                    break;
                }
            }
        }
    }
}

The pointer a points to a memory allocated by C6RUN_MEM_calloc on the ARM-side.

Compiling a binary with c6runlib-cc works, but wenn i try to build a lib out of it, i got this error:

c6runlib-ar rcs libprim.lib libprim.o
"/tmp/024988X0SC9", line 12: error #10008-D: cannot find file
   "/usr/local/ezsdk/component-sources/c6run_0_98_00_00/bin/../lib/c6run_dsp/li
   bc6rundsp_main.a"
error #10008-D: cannot find file
   "/usr/local/ezsdk/component-sources/c6run_0_98_00_00/bin/../lib/c6run_dsp/li
   bc6rundsp.a"
"/tmp/024988X0SC9", line 16: error #10008-D: cannot find file
   "/usr/local/ezsdk/component-sources/c6run_0_98_00_00/bin/../lib/c6run_dsp/c6
   rundsp.cmd"
warning #10210-D: creating ".stack" section with default size of 0x400; use the
   -stack option to change the default size

 undefined             first referenced                                                          
  symbol                   in file                                                               
 ---------             ----------------                                                          
 C6RUN_CACHE_globalInv libprim.dsp_stub.o                                                        
 C6RUN_CACHE_globalWb  libprim.dsp_stub.o                                                        
 C6RUN_CACHE_inv       libprim.dsp_stub.o                                                        
 C6RUN_CACHE_wb        libprim.dsp_stub.o                                                        
 main                  /usr/local/ezsdk/dsp-devkit/cgt6x_7_2_3/lib/rts6740_elf.lib<args_main.obj>

error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "libprim.lib.dsp_image.out"
   not built

Can aanyone help me?

Regards,

Kristian