hi, everyone. I have a question confused me which I used the profiler in CCS3.3 to test a function run time while the result is Incl.average 41xxxxx, and Excl.average is 21xxxxx. the result between Incl.average and Excl.average is huge different, anybody can tell me the possible reason?
also, there is another question, C6747 chip have a feature of 2400 MIPS/1800 MFLOTS, which mean a instruction need only 0.4ns. as we know C6747 CPU clock max is 350Mhz, which means the max clock period is 3ns. the two information are huge different, what reason? know CPU: 6747, CCS:3.3(3.3.82.13), configuration is C67xx simulator.