Other Parts Discussed in Thread: SYSBIOS
When I was trying the jpeg2k demo,
system crash happened when the "while" line below was excuting for the first time in function "ParseContent"
// Stage one: Generate an argc/argv-type list in items[],without comments
// and whitespace.
// This is context insensitive and could be done most easily with lex(1).
while ((unsigned char*)ptr < (unsigned char*)bufend)
{
switch (*ptr)
{
/* Procss whitespace */
case ' ':
.........
the output of console is here:
[C66xx_0]
[C66xx_0]
[C66xx_0] JPEG2000 Encoder: CLASS_C66X
[C66xx_0] 7c0 A7=0x20687470
A8=0x4 A9=0x831094
A10=0x81c818 A11=0x65647400
A12=0x0 A13=0x2
A14=0x65647400 A15=0x0
A16=0x800c24 A17=0x0
A18=0x800bf4 A19=0x20
A20=0x0 A21=0x0
A22=0x0 A23=0x0
A24=0x0 A25=0x7a000000
A26=0x95a56bbc A27=0x95000000
A28=0x95a56bc0 A29=0x4
A[C66xx_0] 30=0x1 A31=0x802230
B0=0x800000 B1=0x834fe8
B2=0x0 B3=0xc048c28
B4=0x15000103 B5=0x4003
B6=0xc0356e4 B7=0x0
B8=0x0 B9=0x0
B10=0x4003 B11=0x834fe8
B12=0x0 B13=0x83
B14=0x835308 B15=0x834fe8
B16=0x61526369 B17=0x2065676e
B18=0x0 B19=0x822128
B20=0x0 B21=0x80[C66xx_0] 19c0
B22=0xf B23=0x0
B24=0x0 B25=0x3000
B26=0x9c B27=0x54
B28=0x5c B29=0x8312a8
B30=0x0 B31=0x831808
NTSR=0x1020d
ITSR=0xf
IRP=0xc0356e4
SSR=0x0
AMR=0x0
RILC=0x0
ILC=0x0
Exception at 0x835050
EFR=0x2 NRP=0x835050
Internal exception: IERR=0x10
Resource conf[C66xx_0] lict exception
ti.sysbios.family.c64p.Exception: line 248: E_exceptionMin: pc = 0x0c0356e4, sp = 0x00834fe8.
To see more exception detail, use ROV or set 'ti.sysbios.family.c64p.Exc[C66xx_0] eption.enablePrint = true;'
xdc.runtime.Error.raise: terminating execution