Other Parts Discussed in Thread: SYSBIOS
Hi,
I am new to SYS/BIOS project. In my project I am going to use Mailbox, tasks, semophores, Memories,Buffers, Timers, SWI,HWI etc.
I want to declare all suing configuration file that is static. I want to use HWIINT14. By using the following parameters I am creating the HWI
Handle: HWIINT
ISR Function: Function1()
Interrupt No: 14
Additional Settings:
Agruments Passed to ISR: 0
Interrupt Priority: 18
Event ID:1
Enable at start up: Enable
Masking option: Self
After entering above details and saving the project I am getting "Hwi 14 already in use (by &ti_sysbios_family_c28_TimestampProvider_rolloverFunc__E). app.cfg /sample ti.sysbios.family.c28.Hwi.Instance#1 XDCTools Configuration Marker"
Can any one usggest any application notes for creating SYS/BIOS project.
Thanks & Regards,
Bhanu Prakash Villuri