Hi all,
We are using DSPLink 1.65.01.06 and TI Arago Linux Kernel version 2.6.32
and DM3730 based embedded board. We need to pass some data between
ARM to DSP of DM3730. Data is first available in the Kernel space of ARM.
Could you please clarify some of my queries?
1. Is it possible to use DSPLink APIs from kernel space (some drivers, kernel modules)
so that we can pass the data directly from kernel space?
2. If so, what are the procedures to be followed? Give some references to documentation telling
usage of DSPLink APIs from kernel space. I think we need to build the DSPLink along with Linux Kernel, right?
3. Or is it mandatory that DSPLink communication possible only between GPP Application and DSP application space?
Thanks in advance,
Honey S