Hi,
I encountered a very strange issue when I did multi-core program development on DSPC8681 platform.
The program should be compiled into one image shared by 8 corepacs on the same DSP. When I load and
run the .out file through my emulator, It can run correctly. But when I load the image through the PCIE interface
with the utilities provided in the desktop-linux-sdk, core 0 will crashed after I load my image into it. For the reason
that I can not get any information about dsp excepte the PC after crashed is locate in function abort(from ccs).
The attached file is my .out file3630.PCIE_proj.rar. and it should be load to 8 corepacs sequentially.
so I want to know how to debug this types of issue...
B.R.
Sunzhao