Hi,
we are working on EVM6670 with CCS 5.2 and pdk 6670 1.1.1.4. We use the PA LLD to send data from the DSP via Ethernet.
QMSS Packets are pushed to PA queue number 5 to add a checksum and contain a route to the EMAC.
We noticed, that when the data rate exceeds a gigabit the PacketDMA does not return/recycle Packets to the FDQ.
Is this problem resulting from the PA being faster than the EMAC?
Is there a workaround or a solution to this problem?
Thaks,
Sebastian