<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="Texas Instruments XDS100v2 USB Emulator_0">
<instance XML_version="1.2" desc="Texas Instruments XDS100v2 USB Emulator_0" href="connections/TIXDS100v2_Connection.xml" id="Texas Instruments XDS100v2 USB Emulator_0" xml="TIXDS100v2_Connection.xml" xmlpath="connections"/>
<connection XML_version="1.2" id="Texas Instruments XDS100v2 USB Emulator_0">
<instance XML_version="1.2" href="drivers/tixds100v2icepick_d.xml" id="drivers" xml="tixds100v2icepick_d.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds100v2cs_dap.xml" id="drivers" xml="tixds100v2cs_dap.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds100v2cortexM.xml" id="drivers" xml="tixds100v2cortexM.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds100v2cs_child.xml" id="drivers" xml="tixds100v2cs_child.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds100v2cortexA.xml" id="drivers" xml="tixds100v2cortexA.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds100v2csstm.xml" id="drivers" xml="tixds100v2csstm.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds100v2etbcs.xml" id="drivers" xml="tixds100v2etbcs.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds100v2pru.xml" id="drivers" xml="tixds100v2pru.xml" xmlpath="drivers"/>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="AM335x_0" href="devices/AM335x.xml" id="AM335x_0" xml="AM335x.xml" xmlpath="devices"/>
<device HW_revision="1" XML_version="1.2" description="AM335x" id="AM335x_0" partnum="AM335x">
<router HW_revision="1.0" XML_version="1.2" description="ICEPick_D Router" id="IcePick_D_0" isa="ICEPICK_D">
<subpath id="subpath_11">
<router HW_revision="1.0" XML_version="1.2" description="CS_DAP Router" id="CS_DAP_M3" isa="CS_DAP">
<subpath desc="M3_wakeupSS_0" id="M3_wakeupSS">
<cpu HW_revision="1.0" XML_version="1.2" desc="M3_wakeupSS_1" description="Cortex_M3 CPU" id="M3_wakeupSS" isa="Cortex_M3"/>
</subpath>
</router>
</subpath>
<subpath id="subpath_12">
<property Type="numericfield" Value="0xc" desc="Port Number_0" id="Port Number"/>
</subpath>
</router>
</device>
</platform>
</connection>
</configuration>
</configurations>
Hi,
I am using the BeagleBone board the following are the details:
1. Board: BeagleBone hardware version: A5A
2. FTDI Chip on the board: FT2232HL
Looks like I have written an erroneous file into the FTDI EEPROM. Because of this I am unable to connect to the target using Code composer studio 5 (CCS5). Please find attached the file I used to write to the EEPROM. Also attached the target configuration file (bbone-target-config.ccxml) used in Code composer studio for your reference. Please let me know if there is anything that I am missing on the configuration OR my eeprom is programmed with incorrect values. This will help me in debugging my programs using the JTAG. Any help/guidance will be highly appreciated.
Please note that I have renamed the attached files as .txt files as I was unable to insert these files as .ept & .ccxml.
Regards,
Shiv