I run u-boot(config base on beagle board) on a board base on omap3530. It get output on uart3, but can't receive anything. Does anybody can help me?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I run u-boot(config base on beagle board) on a board base on omap3530. It get output on uart3, but can't receive anything. Does anybody can help me?
Hi Victor,
I suspect your issue could be due to a hardware problem. I advise you to connect two oscilloscope probe one on uart rx and one on uart tx. The you could observe bits transmission in both destination. This test will determinate whether the problem is hardware or not.
BR
Tsvetolin Shulev