I boot Android ICS Blaze tablet build on my custom board and the LCD starts flickering and i see GFX_FIFO_UNDERFLOW continuously ..
The LCD resolution of 1366*768 ,and the error : omapdss DISPC error: GFX_FIFO_UNDERFLOW, disabling GFX .I modified the sources refer to the http://e2e.ti.com/support/omap/f/849/t/206546.aspx ,it doesn't occur the error but it occur "Unfortunately System UI has stoped " when i clicked OK ,it occur again .
TI Software release reference L27.IS.2.M1_OMAP4_Icecream_Sandwich_Release_Notes