Hi,
I am working on DM6437. i am a beginner with this EVM. can i use the avdsk(automotive vision sdk) to develop an image processing application on TMS320DM6437, instead of dvsdk?. if yes, what is the difference and limitations?
i also want to know how i can intergerate VLib with CCS project to create a simple application which can read the image from an input device, convert it into greyscale image and then display it to the output device.
thanks