Hi,
I have a problem frame skipping when use appro ipnc sdk with ov2710 camera sensor. I found skip one frame when ISR of isif is triggered. exactly speaking, ISR is not triggered for one frame time. then, timestamp would be not gererated. time stamp should be 33ms or 34ms. but, it skipped one frame time stamp each 1.5 ~ 2 seconds.
I looked over vpfe data sheet and am in debugging now. in spite of one week dubugging, I only found isif interrupt not was occured and it skipped one frame.
Please, help me.
BR, Choi