This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x NAND Booting Question

Hello,
I have the following questions about the AM335x Booting.

Can I Boot from NAND Flash memory: MT29F2G08ABAEAWP  (A= Async NAND memory)

On page 4265 (table 26-18) of the document AM335x ARM® Cortex™-A8 Microprocessors  (MPUs)  Technical Reference Manual (spruh73g.pdf),

indicated that the pin GPMC_CLK (Synchronous mode clock) is used in the case of NAND Boot Mode.

At the same time on page 393, have shown links between 16bit (or 8bit) NAND Flash and AM335X. signal, and there, the signal GPMC_CLK not included.

Which of these two statements can  trust, and can I use in this case NAND Flash memory without synchronous clock (in Async mode).

Thanks in advance.