This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ethernet and AM335x

Hello
I want to join to Am335x, Ethernet interface,  using "MII 0" Peripheral Interface port.

In the same pins are located SYSBOOT Configuration Pins also known as: LCD DATA 0 ....15.   

My questions is:

Can I use "MII 0 "  group for Ethernet without problems?
After initialization, the sysboot pull-up or pull-down resistors it will hinder the work of Ethernet communication?

thanks in advance

  • Hello Vladimir,

    Did you have a specific need for the PRU-ICSS subsystem? MII0 is dedicated to this module.

    A majority of our customers use MII1 and/or MII2 as these are connected to the Ethernet switch. Neither of these interfaces share pins with the SYSBOOT options so implementation of either is seamless.

    -DK