This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How can i use DM6437 uart?



now i  use uart on BIOS,  but i dont use PSP libarary, directly config register. But now, when i put a breakpoint in my ISR, the program step into ISR directly after echo.. acturaly i havenot send or receive.  I look up the IFR reg ,it is 0x00008000, ,,

and some use SPBK0,some use UR0FCBK of Dm6437 datasheet  table 3-20

next is my uart_init func,i work with it several weeks, can not find problem:

void UART_INIT()
{
 UART_Handle uart_handle;
    Uint32 divisor = 14; //115200
    EVMDM6437_init(); 
 //sysModuleRegs->VDD3P3VPWDN &=  (~(0x400u)); //UART power up/dont need open Power of flow control
 //sysModuleRegs -> PINMUX0    &= (0x005482A3u);
    //sysModuleRegs -> PINMUX0    |= (0x005482A3u);
 //sysModuleRegs->PINMUX1  &=   (0xFFFFF5FFu);
    //sysModuleRegs->PINMUX1  |=   (0x00000500u); //uart1=bit20:21
 //CFG_PINMUX1 &= 0xFF3FFFFF; //SPBK0
 //CSR &= ~(1<<0); //disable
 //IER &= ~(0x0000FFF3); //disable
 //IER |= 0x01;   //reset interrupt enable
 //ICR = 0xFFFF;
 //ifr = IFR;
 //uart_handle = ( UART_Handle )&UART_MODULE_0;
 UART0_PWREMU_MGMT = 0;
 //_wait( 100 );
 UART0_DLL = ( divisor & 0xff );    // Set baud rate
    UART0_DLH = ( divisor >> 8 ) & 0xff;
 UART0_FCR = 0x0007;        // 4B Clear UART TX & RX FIFOs
    UART0_FCR = 0x0001;        // Enable TX & RX FIFOs  
    UART0_IER = 0x0007;        // Enable interrupts
    UART0_LCR = 0x0003;        // 8-bit words,
    UART0_MCR = 0x0000;        // RTS & CTS disabled,
    UART0_PWREMU_MGMT = 0x6001; // Emulation Free,
 
    IER |= ((1 << 4)|(1<<1)); //int6
    CSR |= 0x01;  //enable                                        // Enable TX & RX componenets 
 //EVMDM6437_UART_open( 0, 115200 );  
 //return;