Hi,
If use GPMC_Wait[0] and GPMC_CS[0] for NOR Flash ,other use GPMC_Wait[1] and GPMC_CS[1] for NAND Flash.
May I ask the
Q1.DSP how to know the Wait [0] & CS [0] connection NOR Flash, wait [1] & CS [1] to connect NAND Flash?
Q2.If the Wait [0] & CS [1] is connected to the NOR Flash or the Wait [1] & CS [0] is connected to the NAND Flash,
whether there will be a problem? DSP How do know?