The AM3517 SOM-M2 module has a Seiko S35390 RTC attached to the I2C-1 interface.
I have some RTC errors during boot up and the /dev entry for the rtc is missing.
I see many others (online) have the same error messages, and many do not. Anyone know of a solution?
"rtc-s35390a 1-0030: error resetting chip"
"rtc-s35390a: probe of 1-0030 failed with error -5
"drivers/rtc/hctosys.c: unable to open rtc device (rtc0)"
dmesg output below:
[ 0.000000] Booting Linux on physical CPU 0
[ 0.000000] Linux version 3.4.15-rt25 (gchiii@genesis) (gcc version 4.5.4 20120305 (prerelease) (GCC) ) #1 PREEMPT RT Tue Nov 20 11:06
:38 EST 2012
[ 0.000000] CPU: ARMv7 Processor [411fc087] revision 7 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
[ 0.000000] Machine: OMAP3517/AM3517 EVM
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] On node 0 totalpages: 65280
[ 0.000000] free_area_init_node: node 0, pgdat c059e9f0, node_mem_map c05ca000
[ 0.000000] Normal zone: 512 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 64768 pages, LIFO batch:15
[ 0.000000] AM3517 ES1.1 (l2cache iva sgx neon isp )
[ 0.000000] Clocking rate (Crystal/Core/MPU): 26.0/332/500 MHz
[ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[ 0.000000] pcpu-alloc: [0] 0
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64768
[ 0.000000] Kernel command line: console=ttyO0,115200n8 ubi.mtd=4 root=ubi0 rootfstype=ubifs rw nohlt rootwait
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 255MB = 255MB total
[ 0.000000] Memory: 252900k/252900k available, 9244k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc051f530 (5214 kB)
[ 0.000000] .init : 0xc0520000 - 0xc0550000 ( 192 kB)
[ 0.000000] .data : 0xc0550000 - 0xc059f3a0 ( 317 kB)
[ 0.000000] .bss : 0xc059f3c4 - 0xc05c95e0 ( 169 kB)
[ 0.000000] NR_IRQS:474
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts
[ 0.000000] Total of 96 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000366] Calibrating delay loop... 483.32 BogoMIPS (lpj=241664)
[ 0.009826] pid_max: default: 32768 minimum: 301
[ 0.010040] Security Framework initialized
[ 0.010131] Mount-cache hash table entries: 512
[ 0.011108] CPU: Testing write buffer coherency: ok
[ 0.011505] Setting up static identity map for 0x803b1550 - 0x803b15a8
[ 0.012969] devtmpfs: initialized
[ 0.017333] omap_hwmod: am35x_otg_hs: cannot be enabled (3)
[ 0.018249] dummy:
[ 0.018707] NET: Registered protocol family 16
[ 0.019134] GPMC revision 5.0
[ 0.019561] ------------[ cut here ]------------
[ 0.019683] WARNING: at arch/arm/mach-omap2/pm.c:48 _init_omap_device+0x3c/0xb4()
[ 0.019683] _init_omap_device: could not find omap_hwmod for iva
[ 0.019714] Modules linked in:
[ 0.019775] [<c0012e18>] (unwind_backtrace+0x0/0xf8) from [<c002a778>] (warn_slowpath_common+0x54/0x64)
[ 0.019805] [<c002a778>] (warn_slowpath_common+0x54/0x64) from [<c002a81c>] (warn_slowpath_fmt+0x30/0x40)
[ 0.019836] [<c002a81c>] (warn_slowpath_fmt+0x30/0x40) from [<c0528ab8>] (_init_omap_device+0x3c/0xb4)
[ 0.019897] [<c0528ab8>] (_init_omap_device+0x3c/0xb4) from [<c0528b74>] (omap2_common_pm_init+0x44/0x5c)
[ 0.019927] [<c0528b74>] (omap2_common_pm_init+0x44/0x5c) from [<c000874c>] (do_one_initcall+0x34/0x174)
[ 0.019958] [<c000874c>] (do_one_initcall+0x34/0x174) from [<c05208a0>] (kernel_init+0x114/0x1c0)
[ 0.019989] [<c05208a0>] (kernel_init+0x114/0x1c0) from [<c000eb8c>] (kernel_thread_exit+0x0/0x8)
[ 0.020019] ---[ end trace 0000000000000001 ]---
[ 0.021789] gpiochip_add: registered GPIOs 0 to 31 on device: gpio
[ 0.021881] OMAP GPIO hardware version 2.5
[ 0.022125] gpiochip_add: registered GPIOs 32 to 63 on device: gpio
[ 0.022430] gpiochip_add: registered GPIOs 64 to 95 on device: gpio
[ 0.022766] gpiochip_add: registered GPIOs 96 to 127 on device: gpio
[ 0.023010] gpiochip_add: registered GPIOs 128 to 159 on device: gpio
[ 0.023284] gpiochip_add: registered GPIOs 160 to 191 on device: gpio
[ 0.024597] error setting wl12xx data
[ 0.024780] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.029022] Reprogramming SDRC clock to 332000000 Hz
[ 0.029052] dpll3_m2_clk rate change failed: -22
[ 0.030456] usbhs_omap: alias fck already exists
[ 0.036682] OMAP DMA hardware revision 4.0
[ 0.045288] bio: create slab <bio-0> at 0
[ 0.046264] vwl1271: override min_uV, 1 -> 1800000
[ 0.046295] vwl1271: override max_uV, 2147483647 -> 1800000
[ 0.046295] vwl1271: 1800 mV
[ 0.046386] reg-fixed-voltage reg-fixed-voltage.1: vwl1271 supplying 1800000uV
[ 0.047424] SCSI subsystem initialized
[ 0.048004] omap2_mcspi omap2_mcspi.1: master is unqueued, this is deprecated
[ 0.048614] omap2_mcspi omap2_mcspi.2: master is unqueued, this is deprecated
[ 0.049163] omap2_mcspi omap2_mcspi.3: master is unqueued, this is deprecated
[ 0.049530] omap2_mcspi omap2_mcspi.4: master is unqueued, this is deprecated
[ 0.050140] usbcore: registered new interface driver usbfs
[ 0.050323] usbcore: registered new interface driver hub
[ 0.050537] usbcore: registered new device driver usb
[ 0.053039] omap_i2c omap_i2c.1: bus 1 rev1.3.12 at 400 kHz
[ 0.053680] omap_i2c omap_i2c.2: bus 2 rev1.3.12 at 400 kHz
[ 0.055908] omap_i2c omap_i2c.3: bus 3 rev1.3.12 at 100 kHz
[ 0.058502] Switching to clocksource 32k_counter
[ 0.061096] cfg80211: Calling CRDA to update world regulatory domain
[ 0.074279] usbhs_omap usbhs_omap: xclk60mhsp1_ck set parentfailed error:-22
[ 0.075286] NET: Registered protocol family 2
[ 0.075683] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.076599] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.076965] TCP bind hash table entries: 8192 (order: 5, 196608 bytes)
[ 0.077484] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.077484] TCP: reno registered
[ 0.077514] UDP hash table entries: 128 (order: 1, 8192 bytes)
[ 0.077575] UDP-Lite hash table entries: 128 (order: 1, 8192 bytes)
[ 0.078033] NET: Registered protocol family 1
[ 0.078613] RPC: Registered named UNIX socket transport module.
[ 0.078643] RPC: Registered udp transport module.
[ 0.078643] RPC: Registered tcp transport module.
[ 0.078674] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.083068] VFS: Disk quotas dquot_6.5.2
[ 0.083190] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.083679] NFS: Registering the id_resolver key type
[ 0.084381] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 0.084991] msgmni has been set to 493
[ 0.086975] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 253)
[ 0.087005] io scheduler noop registered
[ 0.087005] io scheduler deadline registered
[ 0.087097] io scheduler cfq registered (default)
[ 0.087951] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 72) is a OMAP UART0
[ 0.733886] console [ttyO0] enabled
[ 0.738159] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 73) is a OMAP UART1
[ 0.745971] omap_uart.2: ttyO2 at MMIO 0x49020000 (irq = 74) is a OMAP UART2
[ 0.753875] omap_uart.3: ttyO3 at MMIO 0x4809e000 (irq = 84) is a OMAP UART3
[ 0.771514] brd: module loaded
[ 0.780029] loop: module loaded
[ 0.784332] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 0.791595] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xbc (Micron NAND 512MiB 1,8V 16-bit)
[ 0.800659] Creating 5 MTD partitions on "omap2-nand.0":
[ 0.806213] 0x000000000000-0x000000080000 : "xloader-nand"
[ 0.813934] 0x000000080000-0x000000240000 : "uboot-nand"
[ 0.822296] 0x000000240000-0x000000280000 : "params-nand"
[ 0.829559] 0x000000280000-0x000000780000 : "linux-nand"
[ 0.840667] 0x000000780000-0x000020000000 : "jffs2-nand"
[ 1.262573] OneNAND driver initializing
[ 1.267089] UBI: attaching mtd4 to ubi0
[ 1.271148] UBI: physical eraseblock size: 131072 bytes (128 KiB)
[ 1.277740] UBI: logical eraseblock size: 129024 bytes
[ 1.283416] UBI: smallest flash I/O unit: 2048
[ 1.288330] UBI: sub-page size: 512
[ 1.293182] UBI: VID header offset: 512 (aligned 512)
[ 1.299316] UBI: data offset: 2048
[ 2.368194] UBI: max. sequence number: 222
[ 2.388183] UBI: attached mtd4 to ubi0
[ 2.392150] UBI: MTD device name: "jffs2-nand"
[ 2.397827] UBI: MTD device size: 504 MiB
[ 2.403015] UBI: number of good PEBs: 4003
[ 2.407958] UBI: number of bad PEBs: 33
[ 2.412689] UBI: number of corrupted PEBs: 0
[ 2.417358] UBI: max. allowed volumes: 128
[ 2.422241] UBI: wear-leveling threshold: 4096
[ 2.427185] UBI: number of internal volumes: 1
[ 2.431884] UBI: number of user volumes: 1
[ 2.436553] UBI: available PEBs: 0
[ 2.441223] UBI: total number of reserved PEBs: 4003
[ 2.446411] UBI: number of PEBs reserved for bad PEB handling: 40
[ 2.452789] UBI: max/mean erase counter: 2/0
[ 2.457305] UBI: image sequence number: 10075959
[ 2.462249] UBI: background thread "ubi_bgt0d" started, PID 47
[ 2.500305] davinci_mdio davinci_mdio.0: davinci mdio revision 1.5
[ 2.506835] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
[ 2.514404] davinci_mdio.0: probed
[ 2.518035] davinci_mdio davinci_mdio.0: phy[0]: device davinci_mdio-0:00, driver SMSC LAN8710/LAN8720
[ 2.528045] usbcore: registered new interface driver rndis_wlan
[ 2.534393] usbcore: registered new interface driver asix
[ 2.540191] usbcore: registered new interface driver cdc_ether
[ 2.546417] usbcore: registered new interface driver net1080
[ 2.552459] usbcore: registered new interface driver rndis_host
[ 2.558746] usbcore: registered new interface driver cdc_subset
[ 2.565032] usbcore: registered new interface driver zaurus
[ 2.571044] usbcore: registered new interface driver cdc_ncm
[ 2.577362] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.584228] ehci_hcd: block sizes: qh 64 qtd 96 itd 160 sitd 96
[ 2.584411] ehci-omap.0 supply hsusb0 not found, using dummy regulator
[ 3.594268] ehci-omap ehci-omap.0: phy reset operation timed out
[ 3.594329] ehci-omap ehci-omap.0: reset hcs_params 0x1313 dbg=0 cc=1 pcc=3 ordered ports=3
[ 3.594329] ehci-omap ehci-omap.0: reset hcc_params 0016 thresh 1 uframes 256/512/1024 park
[ 3.594390] ehci-omap ehci-omap.0: reset command 0080b02 park=3 ithresh=8 period=1024 Reset HALT
[ 3.594421] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
[ 3.600494] drivers/usb/core/inode.c: creating file 'devices'
[ 3.600524] drivers/usb/core/inode.c: creating file '001'
[ 3.600860] ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
[ 3.608825] ehci-omap ehci-omap.0: park 0
[ 3.609039] ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
[ 3.614990] ehci-omap ehci-omap.0: init command 0010005 (park)=0 ithresh=1 period=512 RUN
[ 3.620452] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
[ 3.626708] usb usb1: default language 0x0409
[ 3.626770] usb usb1: udev 1, busnum 1, minor = 0
[ 3.626800] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 3.633880] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 3.641479] usb usb1: Product: OMAP-EHCI Host Controller
[ 3.647033] usb usb1: Manufacturer: Linux 3.4.15-rt25 ehci_hcd
[ 3.653198] usb usb1: SerialNumber: ehci-omap.0
[ 3.658630] usb usb1: usb_probe_device
[ 3.658660] usb usb1: configuration #1 chosen from 1 choice
[ 3.658721] usb usb1: adding 1-0:1.0 (config #1, interface 0)
[ 3.658966] hub 1-0:1.0: usb_probe_interface
[ 3.658966] hub 1-0:1.0: usb_probe_interface - got id
[ 3.658996] hub 1-0:1.0: USB hub found
[ 3.662963] hub 1-0:1.0: 3 ports detected
[ 3.667175] hub 1-0:1.0: standalone hub
[ 3.667175] hub 1-0:1.0: individual port power switching
[ 3.667205] hub 1-0:1.0: individual port over-current protection
[ 3.667236] hub 1-0:1.0: power on to power good time: 20ms
[ 3.667266] hub 1-0:1.0: local power source is good
[ 3.667297] hub 1-0:1.0: enabling power on all ports
[ 3.667724] drivers/usb/core/inode.c: creating file '001'
[ 3.667877] ehci-omap ehci-omap.0: ...powerup ports...
[ 3.688629] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 3.695098] ohci_hcd: block sizes: ed 64 td 64
[ 3.695312] ohci-omap3 ohci-omap3.0: OMAP3 OHCI Host Controller
[ 3.701568] drivers/usb/core/inode.c: creating file '002'
[ 3.701843] ohci-omap3 ohci-omap3.0: new USB bus registered, assigned bus number 2
[ 3.709838] ohci-omap3 ohci-omap3.0: starting OHCI controller
[ 3.709960] ohci-omap3 ohci-omap3.0: created debug files
[ 3.710174] ohci-omap3 ohci-omap3.0: irq 76, io mem 0x48064400
[ 3.766906] hub 1-0:1.0: state 7 ports 3 chg 0000 evt 0000
[ 3.787017] ohci-omap3 ohci-omap3.0: OHCI controller state
[ 3.787048] ohci-omap3 ohci-omap3.0: OHCI 1.0, NO legacy support registers, rh state running
[ 3.787078] ohci-omap3 ohci-omap3.0: control 0x283 RWC HCFS=operational CBSR=3
[ 3.787109] ohci-omap3 ohci-omap3.0: cmdstatus 0x00000 SOC=0
[ 3.787139] ohci-omap3 ohci-omap3.0: intrstatus 0x00000004 SF
[ 3.787139] ohci-omap3 ohci-omap3.0: intrenable 0x8000005a MIE RHSC UE RD WDH
[ 3.787170] ohci-omap3 ohci-omap3.0: hcca frame #0015
[ 3.787200] ohci-omap3 ohci-omap3.0: roothub.a 0a000203 POTPGT=10 NPS NDP=3(3)
[ 3.787231] ohci-omap3 ohci-omap3.0: roothub.b 00000000 PPCM=0000 DR=0000
[ 3.787231] ohci-omap3 ohci-omap3.0: roothub.status 00008000 DRWE
[ 3.787261] ohci-omap3 ohci-omap3.0: roothub.portstatus [0] 0x00000100 PPS
[ 3.787292] ohci-omap3 ohci-omap3.0: roothub.portstatus [1] 0x00000100 PPS
[ 3.787322] ohci-omap3 ohci-omap3.0: roothub.portstatus [2] 0x00000100 PPS
[ 3.787414] usb usb2: default language 0x0409
[ 3.787445] usb usb2: udev 1, busnum 2, minor = 128
[ 3.787475] usb usb2: New USB device found, idVendor=1d6b, idProduct=0001
[ 3.794677] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 3.802246] usb usb2: Product: OMAP3 OHCI Host Controller
[ 3.807922] usb usb2: Manufacturer: Linux 3.4.15-rt25 ohci_hcd
[ 3.814025] usb usb2: SerialNumber: ohci-omap3.0
[ 3.819366] usb usb2: usb_probe_device
[ 3.819396] usb usb2: configuration #1 chosen from 1 choice
[ 3.819458] usb usb2: adding 2-0:1.0 (config #1, interface 0)
[ 3.819702] hub 2-0:1.0: usb_probe_interface
[ 3.819702] hub 2-0:1.0: usb_probe_interface - got id
[ 3.819732] hub 2-0:1.0: USB hub found
[ 3.823699] hub 2-0:1.0: 3 ports detected
[ 3.827880] hub 2-0:1.0: standalone hub
[ 3.827880] hub 2-0:1.0: no power switching (usb 1.0)
[ 3.827911] hub 2-0:1.0: global over-current protection
[ 3.827941] hub 2-0:1.0: power on to power good time: 20ms
[ 3.827972] hub 2-0:1.0: local power source is good
[ 3.827972] hub 2-0:1.0: no over-current condition exists
[ 3.828002] hub 2-0:1.0: trying to enable port power on non-switchable hub
[ 3.828369] drivers/usb/core/inode.c: creating file '001'
[ 3.828796] usbcore: registered new interface driver cdc_wdm
[ 3.834777] Initializing USB Mass Storage driver...
[ 3.840087] usbcore: registered new interface driver usb-storage
[ 3.846374] USB Mass Storage support registered.
[ 3.851440] usbcore: registered new interface driver libusual
[ 3.857757] usbcore: registered new interface driver usbserial
[ 3.863983] usbcore: registered new interface driver usbserial_generic
[ 3.870910] USB Serial support registered for generic
[ 3.876190] usbserial: USB Serial Driver core
[ 3.880859] usbcore: registered new interface driver ftdi_sio
[ 3.886962] USB Serial support registered for FTDI USB Serial Device
[ 3.893798] ftdi_sio: v1.6.0:USB FTDI Serial Converters Driver
[ 3.900054] usbcore: registered new interface driver ipwtty
[ 3.906005] USB Serial support registered for IPWireless converter
[ 3.912597] usbcore: registered new interface driver keyspan
[ 3.918579] USB Serial support registered for Keyspan - (without firmware)
[ 3.925872] USB Serial support registered for Keyspan 1 port adapter
[ 3.927764] hub 2-0:1.0: state 7 ports 3 chg 0000 evt 0000
[ 3.932739] USB Serial support registered for Keyspan 2 port adapter
[ 3.939422] USB Serial support registered for Keyspan 4 port adapter
[ 3.946228] usbcore: registered new interface driver keyspan_pda
[ 3.952575] USB Serial support registered for Keyspan PDA
[ 3.958374] USB Serial support registered for Keyspan PDA - (prerenumeration)
[ 3.965972] usbcore: registered new interface driver pl2303
[ 3.971862] USB Serial support registered for pl2303
[ 3.977264] usbcore: registered new interface driver usbtest
[ 3.983215] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 3.990112] <6>Waiting for PHY clock good...
[ 4.000976] musb-hdrc: ConfigData=0x1e (UTMI-8, dyn FIFOs, HB-ISO Rx, HB-ISO Tx, SoftConn)
[ 4.001007] musb-hdrc: MHDRC RTL version 1.900
[ 4.001007] musb-hdrc: setup fifo_mode 4
[ 4.001037] musb-hdrc: 28/31 max ep, 16384/16384 memory
[ 4.001281] musb-hdrc musb-hdrc: MUSB HDRC host driver
[ 4.006713] drivers/usb/core/inode.c: creating file '003'
[ 4.007110] musb-hdrc musb-hdrc: new USB bus registered, assigned bus number 3
[ 4.014892] usb usb3: default language 0x0409
[ 4.014953] usb usb3: udev 1, busnum 3, minor = 256
[ 4.014953] usb usb3: New USB device found, idVendor=1d6b, idProduct=0002
[ 4.022094] usb usb3: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 4.029693] usb usb3: Product: MUSB HDRC host driver
[ 4.034942] usb usb3: Manufacturer: Linux 3.4.15-rt25 musb-hcd
[ 4.041046] usb usb3: SerialNumber: musb-hdrc
[ 4.046112] usb usb3: usb_probe_device
[ 4.046142] usb usb3: configuration #1 chosen from 1 choice
[ 4.046203] usb usb3: adding 3-0:1.0 (config #1, interface 0)
[ 4.046386] hub 3-0:1.0: usb_probe_interface
[ 4.046417] hub 3-0:1.0: usb_probe_interface - got id
[ 4.046447] hub 3-0:1.0: USB hub found
[ 4.050415] hub 3-0:1.0: 1 port detected
[ 4.054504] hub 3-0:1.0: standalone hub
[ 4.054534] hub 3-0:1.0: individual port power switching
[ 4.054534] hub 3-0:1.0: no over-current protection
[ 4.054565] hub 3-0:1.0: Single TT
[ 4.054565] hub 3-0:1.0: TT requires at most 8 FS bit times (666 ns)
[ 4.054595] hub 3-0:1.0: power on to power good time: 10ms
[ 4.054626] hub 3-0:1.0: local power source is good
[ 4.054656] hub 3-0:1.0: enabling power on all ports
[ 4.055084] drivers/usb/core/inode.c: creating file '001'
[ 4.055358] musb-hdrc musb-hdrc: USB Host mode controller at d08bc000 using PIO, IRQ 71
[ 4.065673] rtc-s35390a 1-0030: error resetting chip
[ 4.071472] rtc-s35390a: probe of 1-0030 failed with error -5
[ 4.077728] i2c /dev entries driver
[ 4.082672] omap_wdt: OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
[ 4.089996] cpuidle: using governor ladder
[ 4.094329] cpuidle: using governor menu
[ 4.101593] usbcore: registered new interface driver usbhid
[ 4.107513] usbhid: USB HID core driver
[ 4.112426] TCP: cubic registered
[ 4.115905] Initializing XFRM netlink socket
[ 4.120452] NET: Registered protocol family 17
[ 4.125274] NET: Registered protocol family 15
[ 4.129577] mmc0: card claims to support voltages below the defined range. These will be ignored.
[ 4.140319] mmc0: queuing unknown CIS tuple 0x91 (3 bytes)
[ 4.141815] mmc0: new SDIO card at address 0001
[ 4.152343] lib80211: common routines for IEEE802.11 drivers
[ 4.154022] hub 3-0:1.0: state 7 ports 1 chg 0000 evt 0000
[ 4.158416] lib80211_crypt: registered algorithm 'NULL'
[ 4.158447] Registering the dns_resolver key type
[ 4.163574] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1
[ 4.171691] ThumbEE CPU extension supported.
[ 4.179290] voltdm_scale: No voltage scale API registered for vdd_mpu_iva
[ 4.186492] voltdm_scale: No voltage scale API registered for vdd_core
[ 4.193389] PM: no software I/O chain control; some wakeups may be lost
[ 4.201507] clock: disabling unused clocks to save power
[ 4.209228] vwl1271: incomplete constraints, leaving on
[ 4.215423] davinci_emac davinci_emac: using random MAC addr: 36:a2:3c:26:28:3b
[ 4.224243] drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
[ 4.227203] hub 3-0:1.0: state 7 ports 1 chg 0000 evt 0002
[ 4.227264] hub 3-0:1.0: port 1, status 0101, change 0001, 12 Mb/s
[ 4.256561] UBIFS: recovery needed
[ 4.327941] UBIFS: recovery completed
[ 4.331176] hub 3-0:1.0: debounce: port 1: total 100ms stable 100ms status 0x101
[ 4.331909] UBIFS: mounted UBI device 0, volume 0, name "am3517ndu-rootfs"
[ 4.339172] UBIFS: file system size: 256112640 bytes (250110 KiB, 244 MiB, 1985 LEBs)
[ 4.347625] UBIFS: journal size: 9033728 bytes (8822 KiB, 8 MiB, 71 LEBs)
[ 4.355285] UBIFS: media format: w4/r0 (latest is w4/r0)
[ 4.361450] UBIFS: default compressor: lzo
[ 4.365722] UBIFS: reserved for root: 0 bytes (0 KiB)
[ 4.371917] VFS: Mounted root (ubifs filesystem) on device 0:13.
[ 4.378814] devtmpfs: mounted
[ 4.382629] Freeing init memory: 192K
[ 4.433319] usb 3-1: new high-speed USB device number 2 using musb-hdrc
[ 4.558654] usb 3-1: default language 0x0409
[ 4.559020] usb 3-1: udev 2, busnum 3, minor = 257
[ 4.559020] usb 3-1: New USB device found, idVendor=05e3, idProduct=0608
[ 4.570159] usb 3-1: New USB device strings: Mfr=0, Product=1, SerialNumber=0
[ 4.578491] usb 3-1: Product: USB2.0 Hub
[ 4.583160] usb 3-1: usb_probe_device
[ 4.583190] usb 3-1: configuration #1 chosen from 1 choice
[ 4.583557] usb 3-1: adding 3-1:1.0 (config #1, interface 0)
[ 4.583770] hub 3-1:1.0: usb_probe_interface
[ 4.583801] hub 3-1:1.0: usb_probe_interface - got id
[ 4.583801] hub 3-1:1.0: USB hub found
[ 4.588195] hub 3-1:1.0: 4 ports detected
[ 4.592407] hub 3-1:1.0: standalone hub
[ 4.592407] hub 3-1:1.0: individual port power switching
[ 4.592437] hub 3-1:1.0: individual port over-current protection
[ 4.592437] hub 3-1:1.0: Single TT
[ 4.592468] hub 3-1:1.0: TT requires at most 32 FS bit times (2664 ns)
[ 4.592468] hub 3-1:1.0: Port indicators are supported
[ 4.592498] hub 3-1:1.0: power on to power good time: 100ms
[ 4.592987] hub 3-1:1.0: local power source is good
[ 4.592987] hub 3-1:1.0: enabling power on all ports
[ 4.594818] drivers/usb/core/inode.c: creating file '002'
[ 4.595092] hub 3-0:1.0: state 7 ports 1 chg 0000 evt 0002
[ 4.595153] hub 3-0:1.0: port 1 enable change, status 00000503
[ 4.694763] hub 3-1:1.0: port 4: status 0101 change 0001
[ 4.794708] hub 3-1:1.0: state 7 ports 4 chg 0010 evt 0000
[ 4.795013] hub 3-1:1.0: port 4, status 0101, change 0000, 12 Mb/s
[ 4.858001] usb 3-1.4: new high-speed USB device number 3 using musb-hdrc
[ 4.940643] usb 3-1.4: default language 0x0409
[ 4.946411] usb 3-1.4: udev 3, busnum 3, minor = 258
[ 4.946441] usb 3-1.4: New USB device found, idVendor=0bda, idProduct=8189
[ 4.953704] usb 3-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 4.961395] usb 3-1.4: Product: RTL8187B_WLAN_Adapter
[ 4.966705] usb 3-1.4: Manufacturer: Manufacturer_Realtek
[ 4.972351] usb 3-1.4: SerialNumber: 00e04c000001
[ 4.977813] usb 3-1.4: usb_probe_device
[ 4.977844] usb 3-1.4: configuration #1 chosen from 1 choice
[ 4.978698] usb 3-1.4: adding 3-1.4:1.0 (config #1, interface 0)
[ 4.981750] usbserial_generic 3-1.4:1.0: usb_probe_interface
[ 4.981750] usbserial_generic 3-1.4:1.0: usb_probe_interface - got id
[ 4.981964] usbtest 3-1.4:1.0: usb_probe_interface
[ 4.981964] usbtest 3-1.4:1.0: usb_probe_interface - got id
[ 4.983215] drivers/usb/core/inode.c: creating file '003'
>[ 15.104064] udevd[78]: starting version 182
[ 19.476989] rtl8187 3-1.4:1.0: usb_probe_interface
[ 19.477020] rtl8187 3-1.4:1.0: usb_probe_interface - got id
[ 19.715820] ieee80211 phy0: Selected rate control algorithm 'pid'
[ 19.719482] ieee80211 phy0: hwaddr 00:e0:4c:02:72:73, RTL8187BvE V0 + rtl8225z2, rfkill mask 2
[ 19.747375] rtl8187: Customer ID is 0x00
[ 19.755859] Registered led device: rtl8187-phy0::radio
[ 19.758819] Registered led device: rtl8187-phy0::tx
[ 19.763977] Registered led device: rtl8187-phy0::rx
[ 19.764678] rtl8187: wireless switch is on
[ 19.772888] usbcore: registered new interface driver rtl8187