Hello,
I use an external display on the LCD port. With the fixed and default resolution of the BSP (800x480) there is no problem, but when I use 800x600 I have strange artefacts (see attached pictures). This could not be a problem with the display resolution itself, because the mouse will be displayed at every position on the display correctly. But perhaps something with the 2D accelerator configuration (framebuffers)? Seems that the position of the displayed information is on wrong memory positions? The half black file icons on the first picture are from the explorer session before (after closing).
Anyone an idea?
Thanks ahead!