This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is it planned to add USB support in Uboot for TI816XX ??

Hi

I need to use the USB Mass Storage with Uboot on the DM8168 platform.

Today, this feature seems to not be supported with the last release of PSP (04_00_02_14)
I have read some old messages on this forum about USB support in U-Boot. But lots of this messages were left without response.

Do you know if the USB support in Uboot is planned by TI, or if it will be never provided ?

I had a look about source code. It seems necessary to add a low level driver under the MUSB core in Uboot drivers. Like it was done with the EVM365 and OMAP3 platforms.

Maybe this work is already done by another project or another developper ?

Best regards