This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About the MSI interrupt generation in PCIe EP Mode of DM8168.

Guru 10570 points


Hello,
I am evaluating PCIe in DM8168.
On TRM(P1642 17.2.9.2.2), there is description of MSI interrupt generation in EP Mode.

I have understand that the outbound transaction need to be issued for generate the MSI interrupt.
But, on the method 6 of TRM, it seems that the another way exists for generating the MSI interrupt.

The description is following:
6. The Memory Write transaction can also be "optionally" routed through the outbound address translation interface if the destination PCIe address is not directly accessible.

I would like to clarify about meaning of "optinally".
Could you give advise me, please?

- Are there another way to generate MSI interrupt except outbound transaction?

Best regards,
RY
 

  • RY,

    Your understanding on "outbound transaction" is needed to generate MSI is correct.

    Step 6 is really an extension of step 5 where it means that the outbound write can go through address translation if required.

    Consider 2 cases as example:

    A) MSI generation w/ address translation -- this is most likely use case

    1. RC sets MSI address (in EP side register) as 0x60000010
    2. EP side s/w sets outbound translation window size as 8MB each and first window translation for 0x60000000 (i.e., 0x20000000 = 0x60000000 over PCIe)
    3. EP s/w issues a write transaction to address 0x20000010 with MSI data to generate MSI on RC
    4. The above write goes as address translated to 0x60000010 over PCIe and lands on RC side, in turn, generates interrupt

    B) MSI generation w/o address translation

    1. RC sets MSI address (in EP side register) as 0x00000010
    2. EP s/w issues a write transaction to address 0x20000010 with MSI data to generate MSI on RC
    3. The above write goes as address un-translated with MS 4 bits masked (28-bit address range = 256 MB side) as 0x00000010 over PCIe and lands on RC side, in turn, generates interrupt

    As you can see, case A corresponds to step 6, while B is closer to step 5, but I would say the description in TRM should instead mention that the write transaction should be at offset same as MSI address from base of outbound window (0x20000000 + MSI address).

    Note, as we know, in both of the above cases, we have to use one outbound window region to be able to generate MSI and thus I would rather recommend method A where outbound translations are configured always.

  • Hemant.

    Sorry for my late reply.
    Thank you so much for your advice.
    It was helpful for me.

    Best regards,
    RY