Hi all,
I've check some discussions of ti forum, but it seems that there is anything about my question.
I'm working on beagle bone board with ti-sdk-05.04.01.00 and my host pc is working with linux 10.04 lucid lynx ( without virtual machine )
lighttpd is already installed in the target file system . Then it was quite enough changing the lighttpd.conf to comply with my purposes.
( change the index.html directory etc )
Now
, i need to create a new project in code composer with the source code of the lighttpd server (downloaded from lighttpd.net), in order to debug and solve some possible problems.
To do so, i have created a new project in CCSv5 and then add the .c and .h files of the lighttpd .
at this point ... after build project , the "Problems windows" show 294 errors!!
why?!?!
I read the console message and it seems that there are "some" missing file. which ones?
what's wrong with my steps?
thanks in advance!! :)
ps: sorry for my bad english :P