Hello,
did TI plan to support both MACs in a future BSP for EC7, so the second ethernet interface will be usable?
Thanks ahead!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
did TI plan to support both MACs in a future BSP for EC7, so the second ethernet interface will be usable?
Thanks ahead!
Thanks for your answer - but I think, the third party (Adeneo) did not interest at all, if a customer get in touch with them directly and ask whats going on with the second port. (I thought they read the posts in this forum, but apparently no longer - or have other things to-do)
Our board has the second ethernet port and thankfully its supported from the Linux community - I think from your staff.
Greg,
Do you need support for WINCE-7 with dual Ethernet ports supported? If so, we will be able to help you out. Do email me.
Hi Greg,
The current EVM HW does not support both Ethernet connections so the code base could not be verified for multi ETH support. What AM335X HW are you working with? Is it a custom design?
Regards,
I need support dual Ethernet for WINCE 7,Can you help me ? Thanks!
email:853878979@qq.com
Hi, and thanks for your answer. Yes, its a custom design and both network interfaces are working well under Linux.
Now you've also an EVM from TI with which you can use both ethernet interfaces: http://www.ti.com/tool/tmdssk3358?DCMP=dsp-arm-starterkit-120725&HQS=dsp-arm-starterkit-pr-sw1
And I think we're not the only one, that do custom designs and have implemented the second port - you have so much more possibilities with it.