Other Parts Discussed in Thread: SYSBIOS
Hi,
We have a customized DM8148 board running RDK 2.8.
Low power mode is running well, but we have problem in loading DSP firmware in Full Feature mode. Below is the error information:
[m3video] 462684: SYSTEM: Attaching to [DSP] ...
[m3vpss ] 463114: SYSTEM: Attaching to [DSP] ...
[m3video] 463684: SYSTEM: Attaching to [DSP] ...
[m3vpss ] 464114: SYSTEM: Attaching to [DSP] ...
[m3video] 464684: SYSTEM: Attaching to [DSP] ...
[m3vpss ] 465114: SYSTEM: Attaching to [DSP] ...
[m3video] 465684: SYSTEM: Attaching to [DSP] ...
It's stuck at
-----------------------------------------------------------------------------------------------------------------
According to similar symptoms on this forum,
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/162295.aspx
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/163985.aspx
So far we have tried
1) make sure memory map are all matched for DSP, and two M3, no overlapping.
2) uboot files are for full features.
3) update Syslink to syslink_2_20_02_20
Still no luck. We do need some urgent help. Any input is appreciated. Thanks