Hi Experts.
i try to input signal 960H on my costom board.
modifyed hdvpss codes. frame width chang 720 to 960.
HDMI0 and SDTV are grayed out.
Look at the capture driver statistics in system information details on the DEMO program.
[m3vpss ] VIP Parser Reset Count : 0
[m3vpss ]
[m3vpss ] | Total Even Odd Total Even Odd Min / Max Min / Max Dropped Fid Repeat Frame Error Y/C
[m3vpss ] CH | Fields Fields Fields FPS FPS FPS Width Height Fields Count (Desc Error Y/C)
[m3vpss ] ------------------------------------------------------------------------------------------------------------
[m3vpss ] 000 | 294610 147305 147305 125 62 62 65535 / 0 65535 / 0 161045 0 0/0 (294609/0)
[m3vpss ] 001 | 294610 147305 147305 125 62 62 65535 / 0 65535 / 0 161045 0 0/0 (294609/0)
[m3vpss ] 002 | 294610 147305 147305 125 62 62 65535 / 0 65535 / 0 161045 0 0/0 (294609/0)
[m3vpss ] 003 | 294610 147305 147305 125 62 62 65535 / 0 65535 / 0 161045 0 0/0 (294609/0)
[m3vpss ] 100 | 294609 147305 147304 125 62 62 65535 / 0 65535 / 0 161045 0 0/0 (294608/0)
[m3vpss ] 101 | 294609 147305 147304 125 62 62 65535 / 0 65535 / 0 161045 0 0/0 (294608/0)
[m3vpss ] 102 | 294609 147305 147304 125 62 62 65535 / 0 65535 / 0 161045 0 0/0 (294608/0)
[m3vpss ] 103 | 294609 147305 147304 125 62 62 65535 / 0 65535 / 0 161045 0 0/0 (294608/0)
[m3vpss ] 200 | 294608 147304 147304 125 62 62 65535 / 0 65535 / 0 161045 0 0/0 (294607/0)
[m3vpss ] 201 | 294608 147304 147304 125 62 62 65535 / 0 65535 / 0 161045 0 0/0 (294607/0)
[m3vpss ] 202 | 294608 147304 147304 125 62 62 65535 / 0 65535 / 0 161045 0 0/0 (294607/0)
[m3vpss ] 203 | 294608 147304 147304 125 62 62 65535 / 0 65535 / 0 161045 0 0/0 (294607/0)
[m3vpss ] 300 | 294607 147304 147303 125 62 62 65535 / 0 65535 / 0 161045 0 0/0 (294606/0)
[m3vpss ] 301 | 294608 147304 147304 125 62 62 65535 / 0 65535 / 0 161046 0 0/0 (294607/0)
[m3vpss ] 302 | 294608 147304 147304 125 62 62 65535 / 0 65535 / 0 161046 0 0/0 (294607/0)
[m3vpss ] 303 | 294608 147304 147304 125 62 62 65535 / 0 65535 / 0 161046 0 0/0 (294607/0)
Dropped Fields occurs that can be checked.
Can not see the video footage.
Why Drop Field that occurs in addition to the frame size change, modify halgeot to tell me what.
Thanks