This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Antenna interface clock generation circuit of the EVM6474

Hello,

I am interested in using the EVM6474 for OBSAI/CPRI evaluation.

Is there a specific reason why the clock generation circuit for the Antenna
Interface isn't populated, e.g. wouldn't the circuit work as drawn in the
schematics ?

I ask because I am thinking about populating the missing parts on the PCB
(if possible) to make the antenna interface work so that only an external
SFP connected to the AMC connector is required.

Thanks and best regards,
  Dieter