Other Parts Discussed in Thread: AM3358, TPS2041, TPS2041B
Hello,
In the EVM AM3358 baseboard schematics the USB0_DRVNBUS is used to control VBUS of the processor and this processor VBUS connects to the VBUS pin of the USB connector.
I want to use the processor in USB host self powered mode and in additon to use a 4 port hub device. I am using the downstream ports of the hub device to detect an overload condition (hub provides an overload pin and will report it to the host when occurs and this pin connects to a TI TPS2041 device. The output of this device (controlled from hub) enables the power to the external device (based on the OVR condition). So, in this case the hub device provides the power for the VBUS pin for the USB connector.
In this hub case I described above how the USB0_DRVNBUS signals and VBUS power signals of the processor are used and connect so I have a USB self powered host?
Thanks,
Yu-Li