This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP4460 queries



Hi Team,

            Customer was seeking the difference between OMAP4430 and OMAP4460. we have the swpu278d. Except these if there are any other differences then please let me know.

1. Point no 1.3.7 In addition to the two CSI interfaces supported by OMAP4430, OMAP4460 provides a 16-bit parallel camera interface

I think this is saying OMAP4460 is having BT656, 16 bit parallel camera interface as well except two CSI-2 interfaces. Am I right?

 

2-    Point no 2.6: The Video DAC (VDAC) functionality is not supported on OMAP4460. Please elaborate more on it.

Best Regards

Feroz