This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAX chain stops working



I have the following issue with ezsdk 5.05
I have two SDI inputs with 1080p60 signals.
I have configured 3 open max chains.
The first path is encoding the native resolution without any scaling.
The second path is using the same capture but going through deinterlacer before reaching encoder to down scale the 1080p to 720p60.
The third path is using the secondary input and encoding it natively at 720p.
Basically I start these things in sequence and quite often (though not allways) the first two encoders stop working. The first VFCC is not capturing frames anymore after the chain using the second capture is created. I guess the buffers might be held by the DEINT component...

I've attached a UIA log file from start of configuration process to when it dies.

1727.CaptureStoppedWorking.log