Other Parts Discussed in Thread: OMAP-L138
Hi,
I'm using a LCDK OMAP-L138 and CCS v5. I'm using the DSP C674x of the board to do an FFT.
Currently I'm reading data from an external device over SPI with an edma-handler. Then I will do an FFT with that data and send them via UART to an PC.
The reading and sending works well.
Now I want enlarge the program. When N samples of data is sampled i'm cast the data of the external device from int to float to to the FFT (FFT is not implemented yet) while the next N data are sampled.
But now the program crashes sometimes while the sampling and casting or before the sending part. When I'm suspending the program I get for example:
No source available for "0x68000060"
The mapping is:
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
L2 11800000 00040000 00000000 00040000 RWIX
L1P 11e00000 00008000 00000000 00008000 RWIX
L1D 11f00000 00008000 00000000 00008000 RWIX
DDR2 c0000000 08000000 00021152 07fdeeae RWIX
SEGMENT ALLOCATION MAP
Any ideas? Do I use the wrong compiler?
Thanks
Jan