This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ethernet Switch Problem



Hi...

I started a project from the emac-example demo as base. I tested the example sucessfully with internal loopback enabled! After that I tested the example with no Loopback mode: I was able to see the packets send out by the DSP via Wireshark. Now I wanted to test the other direction: I generate packets with a packet builder tool and send them to the destination MAC address, which is defined in the pktMatch test packet. I've also seen this packets with wireshark... but my DSP doesn't reach the receive call-back ISR!

Any help on this?

Regards,

Philipp.