This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sync in analog camera interface in OMAP4460

hi,

I am using the OMAP4460 in my project. i want to use the analog camera for this. while converting the analog camera output (NTSC/PAL) to BT656, i am confused that OMAP4460 support which one syncronization scheme?  in most of the decoder i am having embedded sync and horizontal and vertical sync seperate. on the OMAP4460 datasheet the pin for horizontal and vertical sync is there but i was not able to see the pin for embedde sync. will you please let me know the sync scheme supported on CPI in OMAP4460?

 

with regards,

Ankush agrawal

  • Hi Ankush,

    As per the OMAP4460 TRM, the Parallel Camera Interface (CPI) offers the following features as per the details under Section 8.2.1.1 ISS Interface Features

    Parallel interface (CPI)
    • 16 bits wide
    • up to 148.5 MPix/s
    • BT656 and SYNC mode (HS, VS, FIELD, WEN)

    I hope this clarifies your queries on what sync modes supported by CPI on OMAP4460.

    Thanks & Best Regards,

    Venkat