The C6748 datasheet doesn't specify what capacitors to use with the 32.768kHz crystal. What is the recommendation?
As a side note, the main DSP crystal oscillator says it wants 10-20pF of load capacitance, and the load capacitance is the SERIES combination of C1 and C2. We are using 33pF caps for C1 and C2, which should result in a 16.5pF of load capacitance. Is this correct?
Thanks, Dean