Hi,
I need a xhci host driver used in sys/bois.Can you support me ?
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I need a xhci host driver used in sys/bois.Can you support me ?
Thank you!
Hi cheney liu,
We have several driver packages available depending on the hardware platform and version of BIOS you are using. Please provide this information so that I can further help you.
Steve
Hi Steven
Thank you for r eply!
Our hardware is c667x and the version of BIOS is 6.33.5.46. I think that the xhci is a common interface .We can easy porting the driver if there is a BIOS driver.
Best Regards,
Cheney
Hi cheney liu,
I'm trying to find out some more information about USB support from the drivers team. I've asked them to respond to this thread and they should be getting back to you shortly.
Steve
Hi Steve
Thany you for your reply.I think that the xhci driver is also important for the tusb73x0 user.I can porting the driver from linux,but it is very hard.Because the linux is very complex.If you can offer a xhci driver use in sys/bois ,we can easy to use .If you can offer a xhci driver without os,we can use it also.
Best Regards
Cheney Liu
Cheney Liu,
Latest update - I'm working to track down some SYS/BIOS based drivers for you. However, they would not be XHCI based but instead be OHCI based, as well as for a different hardware platform.
I'll let you know as soon as I have something.
Steve
Hi Steven ,
Thank you for your support .If you have new information about xhci driver,please tell me.I will make this driver by myself now.But I do not have confidence in this project.
Thanks.
Cheney Liu