Hi,
According to AIF2 User Guide, section 3.2.2, for FDD LTE, 15-bit I & 15-bit Q samples are supported. I have checked CPRI spec and it is OK with it :-)
But according to section 7.6 (CPRI input and output module), it states that for the Uplink, data width is 7-bits (for the "efficient" case). Which I think it equals to a resolution of 14 bits per sample, not 15.
So is that right? A 15-bit resolution for the DL and 14-bit resolution for the UL? I would like a confirmation, because I do not understand any clear reasons for this after checking the user guide and the CPRI specification.
Thank you very much in advance.
Regards,
Ricardo