This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How can i configure the dsi register for OMAP 3715



I am working on porting MIPI DSI LCD panel on a custom board with OMAP3715. I am facing problems in clock settings.

From the LCD datasheet, i configure the PCLK as 27MHz., 24BPP, sys_clk=26MHZ, 2 data lane:

clock lane = 27*24/4 = 162MHz

0.75< 26/(RegN + 1)<2.1 --------> REGN=12

 648=2*REGM*26/12+1 ----------->REGM=162

dsi1_pll_fclk = 648/6 = 108 = dsi2_pll_fclk ---------->REGM3=REGM4=5

TxByteClkHS = 648/16= 40.5MHz

Now , i have the proble, how can i calculate DSIFCLK, if DSIFCLK = Clock lan = 162MHZ

how can i calculate VP_PCLK, if it must =27MHZ

how can i make the R=TxByteClkHS/VP_PCLK=2/3.