Other Parts Discussed in Thread: TVP5158
HI
we are developed TI816x (d1 720) dvr product. it works well.
now we are developing 960 product.
960 video capture works well, but screen displayed 720 width.
do you know where to modify or check to display 960 width?
and any patch exists 960 related? , when i finish display swms with 960 , i have to check 960x480(960x576) encoding data and if there is a problem , ask that.
below is my log
thanks.
Best Regards.
[m3vpss ] VIP Parser Reset Count : 0
[m3vpss ]
[m3vpss ] | Total Even Odd Total Even Odd Min / Max Min / Max Average Time Dropped Fid Repeat Frame Error Y/C
[m3vpss ] CH | Fields Fields Fields FPS FPS FPS Width Height Period (Min/Max) Fields Count (Desc Error Y/C)
[m3vpss ] -----------------------------------------------------------------------------------------------------------------------
[m3vpss ] 000 | 15490 7745 7745 60 30 30 960 / 960 240 / 240 16 (16 / 24 ) 1 0 0/0 (0/0)
[m3vpss ] 001 | 15490 7745 7745 60 30 30 960 / 960 197 / 240 16 (16 / 24 ) 1 0 0/0 (0/0)
[m3vpss ] *** [SWMS0] Mosaic Parameters ***
[m3vpss ]
[m3vpss ] Output FPS: 29
[m3vpss ]
[m3vpss ] Win | Ch | Input | Input | Input | Input | Output | Output | Output | Output | Low Cost | SWMS | Data | Blank |
[m3vpss ] Num | Num | Start X, Y | Width x Height | Pitch Y / C | Memory Type | Start X, Y | Width x Height | Pitch Y / C | Memory Type | ON / OFF | Inst | Format| Frame |
[m3vpss ] ----------------------------------------------------------------------------------------------------------------------------------------------------------------------
[m3vpss ] 0 | 0 | 0, 0 | 720 x 240 | 1440 / 1440 | NON-TILED | 0, 0 | 480 x 270 | 3840 / 0 | NON-TILED | ON | 0 | 420SP | OFF |