I want to make sure the transfer rate of TMS320C6678LE PCIe4x using TMDXEVMPCI and WindowsPC.
I purchased and TMS320C6678LE TMDXEVMPCI. PC was set up in WindowsXP32bit them, I can not set some drivers simply labeled [Texas Instruments XDS560 PCI JTAG Emulator] in Device Manager.
Has been set up and is MCSDK2.1.1.4 CCS5.2.1 the PC, it is to the point where you can check sample program can operate in debug connection USB2.0.
What do I do you will have to in order to measure the transfer rate PCIe4x with these? I would need something else or?
Do I need a driver for development and WindowsPC, the creation of applications for transfer rate confirmation WindowsPC?
Please tell me what a good way.