This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Mcspi fifo buffer address

I was looking for MCspi fifo buffer address for DM814x

  • Hello,

    Please, check DM814x TRM, Chapters: 22.3 SPI Registers and 22.3.15 McSPI Channel (i) Transmit Register (MCSPI_TX(i)).

    BR

    Vladimir


  • Hi John,

    The McSPI registers offsets are documented in the DM814x TRM. For example, the McSPI channel 0 FIFO transmit buffer register (MCSPI_TX0) is at offset 0x138.

    The McSPI registers full addresses are documented in the DM814x Datasheet. For example, the McSPI channel 0 FIFO transmit buffer register (MCSPI_TX0) full address is 0x48030138 for McSPI0, 0x481A0138 for McSPI1, 0x481A2138 for McSPI2 and 0x481A4138 for McSPI3.

    Regards,

    Pavel