This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Big algorithm leads to segment distribution error in DVSDK



Hi everybody , I developed a 6446 platform algorithm in CCS,  the algorithm is relatively large, then I put it on DVSDK, which can be compiled and run normally, but when i added more in the algorithm code, probably added about 1/3  of codes,so  the algorithm becomes more complex, then  the compiler error comes as follows:

Board  memory is enough, because I have compiled the same algorithm in the CCS environment , and it can be downloaded into the board and run oK. So it should be  the configuration problem of DVSDK. May I ask how to solve??

there is my content of  .tci file in DSP Server side of DVSDK, maybe usefull

var mem_ext = [
{
    comment:    "DDRALGHEAP: off-chip memory for dynamic algmem allocation",
    name:       "DDRALGHEAP",
    base:       0x88000000,   // 128MB
    len:        0X07A00000,   // 122MB//0X07A00000
    space:      "code/data"
},
{
    comment:    "DDR2: off-chip memory for application code and data",
    name:       "DDR2",
    base:       0X8FA00000,   // 250MB//0X8FA00000
    len:        0X00400000,   //   4MB//0X00400000//26MB
    space:      "code/data"
},
{
    comment:    "DSPLINK: off-chip memory reserved for DSPLINK code and data",
    name:       "DSPLINKMEM",
    base:       0x8FE00000,   // 254MB
    len:        0x00100000,   //   1MB
    space:      "code/data"
},
{
    comment:    "RESET_VECTOR: off-chip memory for the reset vector table",
    name:       "RESET_VECTOR",
    base:       0x8FF00000,   // 255MB
    len:        0x00000080,   // 128 B
    space:      "code/data"
}
];