HI
I want to load Ducati from the shell in 3.4 kernel .Please guide me ow to do so
i was using syslink in 2.6.35 kernel but now icant use as it is deprecated
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
I want to load Ducati from the shell in 3.4 kernel .Please guide me ow to do so
i was using syslink in 2.6.35 kernel but now icant use as it is deprecated
Thanks
Kavith,
I would recommend to start from a TI distribution such as "OMAP Ubuntu Core" (http://omappedia.org/wiki/OMAP_Ubuntu_Core) or "Ubuntu 12.04 Precise Pangolin desktop" (http://omappedia.org/wiki/Prebuilt_ubuntu_binaries). These contain the right version of kernel, kernel modules, ducati firmware, startup scripts, etc. In such distributions, ducati firmware is automatically loaded at bootup and video works off the shelf.
Regards,
-- Olivier
Please note that on 2.6.35 kernel used in Honeycomb and before, syslink daemon was a user space process. In 3.0 onwards syslink driver has moved entirely to kernel. This fundamentally changes the way Ducati is loaded.
Please make sure that kernel config has IPU driver enabled.
Thanks Mayank
I know now it is a Kernel Module.
I want to know Whether on dynamically loading the IPU driver as .ko .Does it reload the Ducati xem3 from firmware folder again
I dont want to re-boot to change the ducati binary everytime
Thanks
Kavitha
syslink driver is built-in the kernel. You can not load/unload it at runtime. Therefore every time Ducati changes, the board needs to be rebooted.